Technical FAQs

Ask a Question

What are the capabilities of the Connexium TCSESM managed switch Ethernet/IP profile?

The Minimum Request Packet Interval (RPI) for Connexium TCSESM managed switch Ethernet/IP profile is 100 ms.
The total number of Ethernet/IP CIP connections to the for Connexium TCSESM managed switch Ethernet/IP profile is 128.
These connections are shared within the Class 1 / Class 3, and are listen-only connections.
Example: If you have 128 Class 1 connections, no further connections are available for Class 3 or listen-only.

Legacy KB System (APS) Data: RESL200210 V2.0, Originally authored by MiMe on 10/10/2009, Last Edited by BrWa on 11/14/2012
Related ranges: ConneXium - Ethernet
Was this helpful?
What can we do to improve the information ?