Technical FAQs

Ask a Question

Do the Connexium TCSESU unmanaged switches support an Ethernet/IP profile?

No, only the Connexium TCSESM managed switches support an Ethernet/IP profile with a 4.1 executive version or greater.


Legacy KB System (APS) Data: RESL200209 V1.0, Originally authored by MiMe on 10/10/2009, Last Edited by MiMe on 10/10/2009
Related ranges: ConneXium - Ethernet
Was this helpful?
What can we do to improve the information ?