Technical FAQs

Ask a Question

Can I connect a Magelis XBTRT511 to a telemacanique M238 PLC?

Yes, you can connect the XBTRT to one of the SL1 or SL2 on the M238 PLC.


Legacy KB System (APS) Data: RESL200147 V1.0, Originally authored by MiMe on 09/30/2009, Last Edited by MiMe on 09/30/2009
Related ranges: Magelis XBT N, R, RT
Was this helpful?
What can we do to improve the information ?