Technical FAQs

Ask a Question

Procedure for canceling a Unity Read_Var transaction

Goals and Symptoms

Procedure for canceling a Unity Read_Var transaction

Causes and Fixes

*** This procedure is intended to cancel a Read_Var transaction in the event the GEST timeout pin in the Read_Var block has not been set and communication is lost to slave device…


Legacy KB System (APS) Data: RESL200143 V1.0, Originally authored by MiMe on 09/30/2009, Last Edited by MiMe on 09/30/2009
Related ranges: Unity Pro
Was this helpful?
What can we do to improve the information ?