Technical FAQs

Ask a Question

Can the Vijeo Citect MBSLAVE driver be used over TCP/IP?

 

 
Frequently asked questions:

No. For use over TCP/IP, you would need to use the MNSLAVE driver.


Legacy KB System (APS) Data: RESL200140 V1.0, Originally authored by MiMe on 09/30/2009, Last Edited by MiMe on 09/30/2009
Related ranges: Vijeo Citect
Was this helpful?
What can we do to improve the information ?