Technical FAQs

Ask a Question

Why are the new IP parameters for a 170ENT11002 not saved to Flash?

Goals and Symptoms

The New IP parameters for a 170ENT11002 are not saved to flash.

Facts and Changes

When an assigned IP, holdup time, or configured IP's is already saved in flash, a Clear Flash Parameters must be initiated first before any new IP, holdup time, or configured IP's are re-entered. This can be accomplished by connecting to the 170ENT1100x device with the Concept Ethernet Configurator and setting it back to BootP.

Causes and Fixes

Flash contains old IP parameters. These need to be cleared.


Legacy KB System (APS) Data: RESL199980 V1.0, Originally authored by MiMe on 09/17/2009, Last Edited by MiMe on 09/17/2009
Related ranges: Modicon Momentum
Was this helpful?
What can we do to improve the information ?