Technical FAQs

Ask a Question

What is the maximum number of Ethernet connections to a 170ENT11001 or a 170ENT11002 ?

Goals and Symptoms

What is the maximum number of Ethernet connections to a 170ENT11001 or a 170ENT11002 ?

Facts and Changes

 

There are a total of 30 connections. 
A maximum of 3 write connections (if more than 1, then they must be configured).
The remaining connections can be for reads. 

Causes and Fixes

No causes or fixes. This is a design criteria.


Legacy KB System (APS) Data: RESL199978 V1.0, Originally authored by MiMe on 09/17/2009, Last Edited by MiMe on 09/17/2009
Related ranges: Modicon Momentum
Was this helpful?
What can we do to improve the information ?