Technical FAQs

Ask a Question

PC locks up when using the ellipsis to choose a variable or FB in Unity Pro.

This usually occurs if dual monitors had been used. Configure the PC for one monitor or reconnect the 2nd monitor and this problem should not occur.


Legacy KB System (APS) Data: RESL199959 V1.0, Originally authored by DaSo on 03/23/2010, Last Edited by DaSo on 03/23/2010
Related ranges: Unity Pro
Was this helpful?
What can we do to improve the information ?