Technical FAQs

Ask a Question

What is the maximum differential pressure ratings on the Magelis XBTGT?

The Magelis XBTGT have a differential pressure rating from 4 inH20 to 7 inH20 (from 10 to 17 hPa or mBar).


Legacy KB System (APS) Data: RESL199726 V1.0, Originally authored by MiMe on 08/27/2009, Last Edited by MiMe on 08/27/2009
Related ranges: Magelis XBT G
Was this helpful?
What can we do to improve the information ?