Technical FAQs

Ask a Question

Can a USB memory stick be used for the web gate instead of the CF card?

No. A CF card is required to use the webgate on the Magelis XBT-GK2330.


Legacy KB System (APS) Data: RESL199725 V1.0, Originally authored by MiMe on 08/27/2009, Last Edited by MiMe on 08/27/2009
Related ranges: Magelis XBT G
Was this helpful?
What can we do to improve the information ?