Technical FAQs

Ask a Question

Are the function keys overlays field replacable?

No. The unit must be sent to the repair center for replacement.


Legacy KB System (APS) Data: RESL199723 V1.0, Originally authored by MiMe on 08/27/2009, Last Edited by MiMe on 08/27/2009
Related ranges: Magelis XBT G
Was this helpful?
What can we do to improve the information ?