Technical FAQs

Ask a Question

Do I need to purchase the Vijeo Historian Control System Connector (part number VJH204320) with a Vijeo Historian system?

Vijeo Historian - Connectors
Vijeo Historian Control System Connector (part number VJH204320) is required when downloading recipe parameters from a SQL database to Vijeo Citect , or uploading batch actuals to a SQL database from Vijeo Citect


Legacy KB System (APS) Data: RESL199719 V1.0, Originally authored by MiMe on 08/27/2009, Last Edited by MiMe on 08/27/2009
Related ranges: Vijeo Historian
Was this helpful?
What can we do to improve the information ?