Technical FAQs

Ask a Question

How can I correct Unity error message 'Invalid range of %IW state ram address was allocated to the 140AVI03000 module at the 1.12 relative topological address'?

You will see this message if a Quantum card, (in this case, in slot 12), is configured for address 0.
Once a valid address is mapped to the I/O card, the Rebuild All should complete without this error.


Legacy KB System (APS) Data: RESL199653 V1.0, Originally authored by DaSo on 08/26/2009, Last Edited by DaSo on 08/26/2009
Related ranges: Modicon Quantum
Was this helpful?
What can we do to improve the information ?