Technical FAQs

Ask a Question

Proworx NXT Status Bar is not completely displayed

There are two Display settings that should be checked.
1/ Control Panel - Display - Settings - Advanced. Make sure that the font size is Normal or Small and that the DPI setting is 96.
2/ Control Panel - Display - Appearance - Advanced. Drop down on Item list. Make sure that the Inactive Title bar is set to 18 or as close to 18 as possible.


Legacy KB System (APS) Data: RESL199608 V1.0, Originally authored by DaSo on 03/23/2010, Last Edited by DaSo on 03/23/2010
Related ranges: ProWORX
Was this helpful?
What can we do to improve the information ?