Technical FAQs

Ask a Question

Is there a way to check the 'save' box on all variables in the Unity Pro Variable Editor at once?

1) Select one variable in the "data editor" and open its "data properties" window.
2) Highlight all the variables in the data editor for which you want to set the "save" attribute.
3) Go back to the "data properties" window of the variable and check the "save" box.
You will find that "save' box is set for all variables that had been highlighted.


Legacy KB System (APS) Data: RESL199465 V1.0, Originally authored by DaSo on 07/28/2009, Last Edited by DaSo on 07/28/2009
Related ranges: Unity Pro
Was this helpful?
What can we do to improve the information ?