Technical FAQs

Ask a Question

Is there a dummy filler module for the M340 rack?

If a position is unoccupied on a rack, you are advised to install a BMX XEM 010 cover in this slot, in order to protect it. The cover is installed and attached to the rack like a narrower version of an normal module.
You are advised to use this cover on each unoccupied position on the rack to comply with the IP20 Protection Index. BMX XEM 010 covers are sold in sets of 5.


Legacy KB System (APS) Data: RESL199300 V1.0, Originally authored by DaSo on 07/08/2009, Last Edited by DaSo on 07/08/2009
Related ranges: Modicon M340
Was this helpful?
What can we do to improve the information ?