Technical FAQs

Ask a Question

Does the XBTGT series have a Class 1 Div 2 certification?

Yes the XBTGT line is Class 1 Div 2 T4A or T5 (UL and CSA) Certified,


Legacy KB System (APS) Data: RESL199265 V1.0, Originally authored by GeMc on 07/01/2009, Last Edited by GeMc on 07/01/2009
Related ranges: Magelis XBT GT
Was this helpful?
What can we do to improve the information ?