Technical FAQs

Ask a Question

I get the following error message when trying to run OFS: "NA_UTIL not found. NetAccess may be damaged or not installed" What could be the cause?


The OFS V3.0 driver link has changed and it now use Netaccess interface.

Netaccess is a new interface. Basically all drivers seen from OFS or other application using Netaccess open a socket like TCP/IP and then link to the driver.

To solve this error, install driver manager and the problem/message will go away.


Legacy KB System (APS) Data: RESL199262 V1.0, Originally authored by MiMe on 06/30/2009, Last Edited by MiMe on 06/30/2009
Related ranges: OPC Factory
Was this helpful?
What can we do to improve the information ?