Technical FAQs

Ask a Question

What are the part numbers for the Modicon M238 PLC?

The part numbers for the Modicon M238 PLC are;
TM238LFDC24DT
TM238LDD24DT

 
Reference Power Supply Serial Ports CANopen Master Discrete Inputs Discrete Outputs Memory size
TM238LFDC24DT
24 Vdc
SL1: RS232/RS485
SL2: RS485
Yes
8 fast inputs(1)
+
6 standard inputs
4 transistor fast outputs(2)
+
6 transistor standard outputs
2 MB
TM238LDD24DT
24 Vdc
SL1: RS232/RS485
No
1 MB

Legacy KB System (APS) Data: RESL199250 V2.0, Originally authored by DiSa on 06/29/2009, Last Edited by BrWa on 07/06/2012
Related ranges: Modicon M238
Was this helpful?
What can we do to improve the information ?