Technical FAQs

Ask a Question

What is the Default IP address of the Ethernet port on the W@de W315/W320E ?

The Default IP address of the Ethernet port on the W@de W315/W320E is IP address - 172.16.0.5


Legacy KB System (APS) Data: RESL199244 V1.0, Originally authored by MiMe on 06/27/2009, Last Edited by MiMe on 06/27/2009
Related ranges: ConneXium - Ethernet, W@de RTU
Was this helpful?
What can we do to improve the information ?