Technical FAQs

Ask a Question

In Vijeo Designer V5.0, what Rockwell file extension can I use to link the variables?

Vijeo Designer V5.0 supports Rockwell RSLogix5000 *.L5K symbol file for linking variables.


Legacy KB System (APS) Data: RESL199038 V1.0, Originally authored by GeMc on 05/29/2009, Last Edited by GeMc on 05/29/2009
Related ranges: Vijeo Designer
Was this helpful?
What can we do to improve the information ?