Technical FAQs

Ask a Question

What are the new Twido I/O module part numbers and what I/O modules do they replace?

Goals and Symptoms

To give matrix on the old part number for the Twido I/O and give new replacement numbers.

Causes and Fixes

Below is the matrix of the old numbers and the new replacement numbers.


Twido was obsoleted 12/31/2016 and was replaced by the M221 family. The M221 will support the TM2 modules and the new TM3 modules in the same configurationi but not the TWD modules.
Was this helpful?
What can we do to improve the information ?