Technical FAQs

Ask a Question

What does a -1603 error indicate in Concept?

This error usually occurs when trying to go online to a PLC and is usually caused by one of the following:
1/ Expansion Size in Peer Cop needs to be decreased. This must be done offline.
2/ If it is a Hot Standby system, either no CHS or HSBY loadable configured or heap size is too large.
3/ Memory partitions maybe incorrect or may be illegal for controller type.


Legacy KB System (APS) Data: RESL1987 V1.0, Originally authored by on , Last Edited by on
Related ranges: Concept
Was this helpful?
What can we do to improve the information ?