Technical FAQs

Ask a Question

Release Notes for 'BMXNOE0100' exec firmware version 2.0.

Goals and Symptoms

Release Notes for the 'BMXNOE0100' exec firmware version 2.0.

Facts and Changes

'BMX NOE 0100' exec firmware version 2.0

Causes and Fixes

The following new features and enhancements have been added in version 2.0:

  • The ability to configure the 'BMXNOE100' for NTP.
  • The ability to have two (2) NOEs configured in the same rack.
  • The ability to use the DATA_EXCH function block with the 'BMXNOE100'
The following problems have been fixed in version 2.0:
  • The 'Unity Loader' fails to download the exec firmware to the BMXNOE100
  • The 'BMXNOE100' cannot communicate to more than 16 devices using the Read_Var or
Write_Var function block.
 

Legacy KB System (APS) Data: RESL198532 V1.0, Originally authored by AlCh on 05/20/2009, Last Edited by AlCh on 05/20/2009
Related ranges: Modicon M340
Was this helpful?
What can we do to improve the information ?