Technical FAQs

Ask a Question

How to find the 'IO Scanner' health status bit in a PL7 application.

Goals and Symptoms

How to find the 'IO Scanner' health status bit in a PL7 application.

Facts and Changes

All Premium PLC's using PL7.

Causes and Fixes

The following steps will show how to find and use the health bit for the IO Scanner in PL7.

  • This example uses an ETY5103 configured in slot 2 of the Premium rack.
  • Two IO scanner entries are configured in the ETY5103 'Scanned peripherals' table..


To find the health bit for the IO Scanner:
  • Double click on IO to open the Variables window.

 
  • Click on the down arrow and select the 'TSXETY5103' module from the drop down list.

 
  • The words representing the IO scanner channels will be listed as '%IWx.0.1' through %IWx.0.2. In
this example, it is shown as '%IW2.0.1' through '%IW2.0.2'.

 
  • When the IO Scanner is healthy, the debug screen shows the respective bit for the IO Scanner
channel as green.
  • The animation table shows the respective bits of the %IW2.0.1 word is with a value of 1.

 
  • When the IO Scanner is unhealthy, the debug screen shows the respective bit for the IO Scanner
channel as red.
  • The animation table shows the respective bit of the %IW2.0.1 word is with a value of 0.


The health bit for the 64 'IO Scanner' lines listed in the 'Scanned peripherals' table can be
referenced from within logic by using the address %IW2.0.1:X0 through %IW2.0.1:X15 and %IW2.0.2:X0
through %IW2.0.2:X15





 

Legacy KB System (APS) Data: RESL198513 V1.0, Originally authored by AlCh on 06/11/2009, Last Edited by AlCh on 06/11/2009
Related ranges: Modicon Premium
Was this helpful?
What can we do to improve the information ?