Technical FAQs

Ask a Question

How do you resolve the error "Regsvr32error on\AS_DC33_TwidoWorkShop" that gets reported when installing TwidoSuite?

Goals and Symptoms

Software Installation issue

Causes and Fixes

This is the procedure to solve the Regsvr32error on\AS_DC33_TwidoWorkShop error:
1) Menu START--->> RUN menu




2) Type "msconfig" and hit OK



3) Select "Diagnostic Start up" and apply



4) Restart PC

5) Install Twido Suite

6) After installation modify the msconfig back to Normal Startup.


 


Legacy KB System (APS) Data: RESL198413 V1.0, Originally authored by TVe on 05/01/2009, Last Edited by TVe on 05/01/2009
Related ranges: TwidoSuite
Was this helpful?
What can we do to improve the information ?