Technical FAQs

Ask a Question

What are the part numbers for the low cost Telefast sub-base for the M340 discrete input / output modules?

Given below are the part numbers for the low cost sub-base:


Legacy KB System (APS) Data: RESL198410 V1.0, Originally authored by TVe on 05/01/2009, Last Edited by TVe on 05/01/2009
Related ranges: Modicon M340, Advantys Telefast ABE7
Was this helpful?
What can we do to improve the information ?