Technical FAQs

Ask a Question

'Error obj = clsNavlist.cls' is returned when starting 'ProWORx 32'

Goals and Symptoms

'Error obj = clsNavlist.cls' is returned when starting 'ProWORx 32'.

Facts and Changes

'ProWORX 32'...all versions.

Causes and Fixes

If the default 'Projects' folder is corrupted, the error message 'Error obj = clsNavlist.cls' could
appear when starting 'ProWORx 32'.

The issue can be resolved by using the following steps:

  • Locate and open the 'ProWORX 32' installation folder (i.e., c:\ProWORX\32).
  • Rename the 'project' folder to a different name (i.e., old_project, etc.).
  • Start 'ProWORX 32'.

Legacy KB System (APS) Data: RESL198381 V1.0, Originally authored by AlCh on 04/29/2009, Last Edited by AlCh on 04/29/2009
Related ranges: ProWORX
Was this helpful?
What can we do to improve the information ?