Technical FAQs

Ask a Question

How many simultaneous Modbus TCP/IP connections does the Twidoport support?

The Twidoport, 499TWD01100, supports up to 6 (six) simultaneous Modbus TCP/IP connections.


Legacy KB System (APS) Data: RESL198159 V1.0, Originally authored by TVe on 03/31/2009, Last Edited by TVe on 03/31/2009
Related ranges: Twido
Was this helpful?
What can we do to improve the information ?