Technical FAQs

Ask a Question

How do I create a new connection in Twido Suite?

Goals and Symptoms

Steps to help create a new connection with the PLC

Causes and Fixes

To create a new connection in Twido Suite, you need to follow these steps:
1) Select the Manage connection.



2) Add a new connection




3) Create the new connection


Legacy KB System (APS) Data: RESL198156 V1.0, Originally authored by TVe on 03/31/2009, Last Edited by TVe on 03/31/2009
Related ranges: TwidoSuite
Was this helpful?
What can we do to improve the information ?