Technical FAQs

Ask a Question

Given a choice to execute the PIDFF block using a Periodic task or the SAMPLETM block which would offer the most reliable means to execute PIDFF? SAMPLETM or the Periodic Task?

The function block SAMPLETM is used to enable some logic (e.g. the PID function block) in dedicated time intervals. This was necessary with the Concept Low End CPUs because these CPUs don't allow to use interrupt sections. Concept High End CPUs (434, 534) and Unity CPUs allow time interrupt sections and Fast Tasks.
Therefore, it is not necessary to use the SAMPLETM block when using Concept High End CPUs (434, 534) and Unity CPUs


.


Legacy KB System (APS) Data: RESL198149 V1.0, Originally authored by MiMe on 03/27/2009, Last Edited by MiMe on 03/27/2009
Related ranges: Unity Pro
Was this helpful?
What can we do to improve the information ?