Technical FAQs

Ask a Question

How can I get the diagnostic file information if my Magelis XBT-GT gets a Java Exception runtime error?

In a rare circumstance that a Java Exception error is generated on the Magelis XBT-GT. A diagnostics log file can be found on the CF card.
The path of the file on the CF card is::
<root drive>\PUBLIC\PROJECT\<TargetName>\DATA\FATALERR\ERRORLOG.TXT


Legacy KB System (APS) Data: RESL198147 V1.0, Originally authored by MiMe on 03/27/2009, Last Edited by MiMe on 03/27/2009
Related ranges: Magelis XBT G
Was this helpful?
What can we do to improve the information ?