Technical FAQs

Ask a Question

MTBF for the 499TWD01100.

Goals and Symptoms

MTBF for the 499TWD01100.

Facts and Changes

499TWD01100.

Causes and Fixes

The following MTBF numbers are for the 499TWD01100.

MTBF 30° Continuous 5480323 hrs.
MTBF 30° Intermittent 3456010 hrs.
MTBF 60° Continuous 3791742 hrs.
MTBF 60° Intermittent 2748604 hrs.
MTBF 85° Continuous 1850683 hrs.
MTBF 85° Intermittent 1571312 hrs.


Was this helpful?
What can we do to improve the information ?