Technical FAQs

Ask a Question

Changing the 'Power Flow Lne Width' causes 'ProWORX 32' to close.

Goals and Symptoms

Changing the 'Power Flow Lne Width' causes 'ProWORX 32' to close.

Facts and Changes

ProWORX 32 version 2.1, Service Pack

Causes and Fixes

Changing the 'Power Flow Lne Width' using the up or down arrows in the Logic Properties window
causes 'ProWORX 32' to close.


The following workaround can be used to change the line width without using the up or down arrows:

  • Click on the textbox next to the 'Power Flow Line Width' to highlight the text..
  • Change the value within the textbox to a number between 1 and 6.
  • Click on the 'Apply button.
  • Click on 'OK' to close the properties window.


This problem has been fixed in Patch A for Service Pack 1. Patch A is expected to be released near the end of Q2/09.




 

Note: Proworx software was obsoleted 12/31/2016 and upgrading to he new hardware and Unity Pro is recommended.
Was this helpful?
What can we do to improve the information ?