Technical FAQs

Ask a Question

How do you delete a subroutine from a TwidoSuite program?

Goals and Symptoms

Show steps to delete subroutine form TwidoSuite program.

Causes and Fixes

When in a program that has a subroutine that you want to delete you will need to do the following steps.
Go to where there is a subroutine in the program as below shows.





Once highlighted, hit the delete key on your keyboard and it will delete the subroutine from the program. You then need to save the program.


Legacy KB System (APS) Data: RESL198046 V1.0, Originally authored by DiSa on 03/16/2009, Last Edited by DiSa on 03/16/2009
Related ranges: TwidoSuite
Was this helpful?
What can we do to improve the information ?