Technical FAQs

Ask a Question

Can I expand the RAM memory on my Magelis Compact iPC MPCKT22NAA00N?

Yes. The Ram can be extanded up to 1024MB. To add an additional 512MB memory you would need to purchase MPCYK05RAM512.


Legacy KB System (APS) Data: RESL197896 V1.0, Originally authored by MiMe on 02/25/2009, Last Edited by MiMe on 02/25/2009
Related ranges: Magelis Compact iPC
Was this helpful?
What can we do to improve the information ?