Technical FAQs

Ask a Question

Is there a fiber optic distance requirement between the 140CHS11000 modules in a Quantum Hot Standby System?

The fiber optic distance requirement between the 140CHS11000 modules is 3 meters which is the length of the supplied fiber cable.
A maximum distance can be up to 1km using 62.5/125 micrometer fiber cable with ST style connectors.

Legacy KB System (APS) Data: RESL197850 V2.0, Originally authored by DiSa on 02/18/2009, Last Edited by DiSa on 11/15/2012
Related ranges: Modicon Quantum
Was this helpful?
What can we do to improve the information ?