Technical FAQs

Ask a Question

What software tool is used for downloading the configuration to a 140NOL91110.

Goals and Symptoms

What software tool is used for downloading the configuration to a Quantum 140NOL91110 module.

Facts and Changes

140NOL91110

Causes and Fixes

The Configuration Tool was included in the same shipping box for the 140NOL91110 module.

The Configuration Tool is a third party network configuration tool that must be purchased
from Metravision. It is needed for mapping the network variables form the Configuration Tool used
with the LonWORKs network devices.

Note: The 140NOL91110 was discontinued back around 1999-2000 and it is considered to be obsolete.


Legacy KB System (APS) Data: RESL197654 V1.0, Originally authored by AlCh on 12/09/2010, Last Edited by AlCh on 12/09/2010
Related ranges: Modicon Quantum
Was this helpful?
What can we do to improve the information ?