Technical FAQs

Ask a Question

Supported operating systems for 'ProWORX NxT' and 'ProWORX 32'

Goals and Symptoms

Supported operating systems for 'ProWORx NxT' and 'ProWORX 32'.

Facts and Changes

'ProWORX NxT' and 'ProWORX 32'

Causes and Fixes


The following table describes what operating system will support either 'ProWORx NxT' or
'ProWORX 32'.



Note: 1.) Requires 'ProWORX 32 version 2.1, Service Pack 1.

2.) 'ProWORx NxT' is a 16 bit Windows application and it will not work on Microsoft Vista
or any newer operating system.


 


Legacy KB System (APS) Data: RESL196863 V2.0, Originally authored by AlCh on 01/22/2009, Last Edited by AlCh on 07/15/2010
Related ranges: ProWORX
Was this helpful?
What can we do to improve the information ?