Technical FAQs

Ask a Question

How Can I insert and manage Advantys island in Unity PLC based control system?

In the attached 'How Can I...' document one can find the following:
Advantys island can be connected to Unity PLC based architecture using UAG.
The variables will be assigned to the IOs from Advantys island.

How Can I manage Advantys Island.pdf


Legacy KB System (APS) Data: RESL196792 V1.0, Originally authored by HeWE on 01/10/2009, Last Edited by HeWE on 01/10/2009
Related ranges: Unity Application Generator (UAG)
Was this helpful?
What can we do to improve the information ?