Technical FAQs

Ask a Question

How Can I exchange data between TWIDO PLC and any Unity PLC using UAG

In the attached 'How Can I...' document one can find the following:
In UAG it can be configured to exchange data between TWIDO PLC over Modbus TCP with any Unity PLC. The TWIDO has to communicate over IO Scanner.

How Can I communicate data with TWIDO PLC using UAG.pdf


Legacy KB System (APS) Data: RESL196790 V2.0, Originally authored by HeWE on 01/10/2009, Last Edited by HeWE on 01/13/2009
Related ranges: Unity Application Generator (UAG)
Was this helpful?
What can we do to improve the information ?