Technical FAQs

Ask a Question

How Can I manage devices over Profibus?

In the attached 'How Can I...' document one can find the following:
In UAG, the user can configure Profibus using ProSoft/SyCon tool for Quantum and Premuim PLCs.
UAG offers a possibility to include devices connected to PLC over Profibus and makes it available so that IO variables can be used in control modules.

How Can I manage Profibus based devices.pdf


Legacy KB System (APS) Data: RESL196782 V2.0, Originally authored by HeWE on 01/08/2009, Last Edited by HeWE on 01/09/2009
Related ranges: Unity Application Generator (UAG)
Was this helpful?
What can we do to improve the information ?