Technical FAQs

Ask a Question

How Can I develop a new SCoD using properties of an existing SCoD?

In the attached 'How Can I...' document one can find the following:
In UAG a new SCoD can be developed by copying an existing SCoD, so that all the properties of an existing SCoD can be used.

How Can I develop new SCoD using an existing one.pdf


Legacy KB System (APS) Data: RESL196780 V2.0, Originally authored by HeWE on 01/08/2009, Last Edited by HeWE on 01/09/2009
Related ranges: Unity Application Generator (UAG)
Was this helpful?
What can we do to improve the information ?