Technical FAQs

Ask a Question

How Can I change interface with DFB: Adding/deleting a pin?

In the attached 'How Can I...' document one can find the following:
A SCoD is developed and committed, obviously with a Unity DFB.
How can I change the interface, i.e. I want to add /delete a pin?

How Can I change interface with DFB.pdf


Legacy KB System (APS) Data: RESL196779 V2.0, Originally authored by HeWE on 01/08/2009, Last Edited by HeWE on 01/09/2009
Related ranges: Unity Application Generator (UAG)
Was this helpful?
What can we do to improve the information ?