Technical FAQs

Ask a Question

How Can I develop a generic device which can communicate over IO Scanner?

In the attached 'How Can I...' document one can find the following:
In UAG new devices can be included by defining them under Customization.
There are different methods of communication and rack types possible.

How Can I develop a generic device.pdf


Legacy KB System (APS) Data: RESL196778 V2.0, Originally authored by HeWE on 01/08/2009, Last Edited by HeWE on 01/09/2009
Related ranges: Unity Application Generator (UAG)
Was this helpful?
What can we do to improve the information ?