Technical FAQs

Ask a Question

How Can I key-in constant value to a Unity Pro variable from UAG?

In the attached 'How Can I...' document one can find the following:
In UAG a SCoD can be developed in such a way that literals for Unity Pro can be defined as properties of a Control Module.

How Can I key in constant from a SCoD into Unity DFB.pdf


Legacy KB System (APS) Data: RESL196776 V2.0, Originally authored by HeWE on 01/08/2009, Last Edited by HeWE on 01/09/2009
Related ranges: Unity Application Generator (UAG)
Was this helpful?
What can we do to improve the information ?