Technical FAQs

Ask a Question

Why is the option to insert an equation network grayed out in ProWORX 32 v2.1?

The equation network option will only be grayed out when creating a new ProWORX 32 project. If there's no other logic in the program, the Equation Network feature will be greyed out. Once you insert any instruction into Network 1 of the logic, the Equation Network feature will be activated. If Network 1 is going to be an equation network, simply delete the instruction and the equation network feature is now activated.


Legacy KB System (APS) Data: RESL194520 V3.0, Originally authored by RoAl on 12/23/2008, Last Edited by RoAl on 11/22/2012
Related ranges: ProWORX
Was this helpful?
What can we do to improve the information ?