Technical FAQs

Ask a Question

What is the difference between Momentum I/O bases 170ANR12090 and 170ANR12091?

The 170ANR12091 is similiar to the model 170ANR12090, with the exception that it has bipolar analog input and output ranges of -10 to +10 V, instead of unipolar ranges of 0-10 V.


Legacy KB System (APS) Data: RESL193347 V1.0, Originally authored by DaSo on 12/11/2008, Last Edited by DaSo on 12/11/2008
Related ranges: Modicon Momentum I/O
Was this helpful?
What can we do to improve the information ?