Technical FAQs

Ask a Question

Error message 'Error when opening the project file'

Goals and Symptoms

You Open the .STU file and get the error message   'Error when opening the project file'.

Facts and Changes

UnityPro V4.0 or older.

Causes and Fixes

This error happens, if in the NOM configuration the communication type 'DIO Bus'  is marked, but no DIO drops are configured. The problem is fixed with UnityPro V4.1. In older UnityPro versions you should avoid a marked 'DIO Bus' without DIO drops configured.


Legacy KB System (APS) Data: RESL193195 V1.0, Originally authored by KlSP on 11/20/2008, Last Edited by KlSP on 11/20/2008
Related ranges: Unity Pro
Was this helpful?
What can we do to improve the information ?