Technical FAQs

Ask a Question

Can I use the TSXCUSBMBP Modbus Plus adapter with Vijeo Designer v4.6 in simulation build mode?


Vijeo Designer V4.6 in simulation build supports TSXCUSBMBP Modbus Plus adapter.

It does not support the SA85 or PCI MB+ adapter. The Modbus Plus driver must be installed on the PC separately.


Legacy KB System (APS) Data: RESL193051 V1.0, Originally authored by MiMe on 10/28/2008, Last Edited by MiMe on 10/28/2008
Related ranges: Vijeo Designer
Was this helpful?
What can we do to improve the information ?